Examples of successful applications in shipbuilding

Corrosion-free ball bearings for wingsails

bound4blue supplies automatic wind-assisted propulsion systems (wingsails) for ship owners and operators who want to use renewable energies and reduce fuel costs and pollutant emissions by up to 40 per cent. Use at open sea requires components that can withstand severe weather conditions.

More about the application
bound4blue wingsail
bound4blue wingsail

Highly resilient plain bearings for hinges in shipbuilding

Heavy doors are installed on yachts in the gunwale area with an opening angle of 180°. Their hinges must allow high loads and be corrosion-free. But previous solutions were often very susceptible to corrosion and wear near the pivot points. iglidur plain bearings were able to correct the problems of the previous design. The hinges are now completely maintenance-free.

More about the application
hinges in shipbuilding
shipbuilding hinges

No problem with salt water: rod ends in the rowing rods

The award-winning sailing boat Seascape 24 is a performance-oriented fast small cruiser with which you can also go on a leisurely trip. The steering system is a double oar design, which allows complete control even at high speeds. To ensure that the double oar steering works reliably, the designers use igubal KARM plastic rod ends for the connections.

More about the application
rod ends in the small cruiser
rod ends in the small cruiser


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH