LED bulbs production with cobots

Problem

  • Very small radius of movement
  • System size should not be significantly increased by the structure
  • When moving the cobot without energy supply, the cables were bent too strongly and unpredictably.
  • The maintenance options were limited
  • The cobot could not utilise its full movement potential without a defined energy supply.

Solution

  • No line problems, as these are protected by undefined.
  • Increased stability of the entire system
  • The cobots move much more evenly across the entire working area
  • Line protection in the event of contact between the cobots due to incorrect programming is avoided.