Fail-safe energy chain as cable guidance in an innovative bicycle garage

The storage and retrieval unit for parking the bicycles works reliably thanks to the E2.1 e-chain.

An innovative idea in times of climate change: to simplify CO2-free mobility in inner cities, the French company SERAAP has developed a bicycle garage. The special feature: a storage and retrieval unit inside the garage picks up the bicycle and places it in a defined place - which can sometimes be several metres high. The machine specialist relies on our E2.1 series energy chain systems for guiding the energy and data cables. 

Profile

  • What was needed: E2.1 series energy chains
  • Requirements: Safe and reliable cable guidance, high flexibility, travel speeds of up to 1m/s
  • Industry: Storage and retrieval units in material handling
  • Success for the customer: With the E2.1 e-chain for medium loads, the customer saves costs twice: when purchasing and when filling with cables quickly and easily. In this way, SERAAP was able to meet the price defined by the customer.
Discover all products for material handling
Bicycle garage by SERAAB With modular and automated garages in large cities, SERAAB creates new and space-saving parking options for bicycles.

Problem

Initially with a focus on special machines and later increasingly also on robotics, the French company SERAAP has established itself as an innovative machine manufacturer. Customers commission the company, for example, to automate processes and make them more cost-effective.
The bicycle garage developed by SERAAP, which is intended to make mobility in large cities even more convenient, can also be described as innovative. The idea is to create a space-saving parking area with modular, cube-shaped bicycle sheds for as many bicycles as possible in every city with a population of 100,000 or more. A project in the spirit of climate change.
After the bike owner has reserved a space via an app, he receives a code on his cell phone, which he can enter to use the garage. When the bike is parked and locked, sensors start checking the dimensions of the bike. A storage and retrieval unit picks it up and places it in the reserved position. This can sometimes be several metres high.

Solution

For the implementation of the bicycle garage, a solution for the safe energy supply of the storage and retrieval unit was also needed. Because it had to move freely within the cube without the data and energy cables restricting or slowing down the movement of the robot. While the SRU pulls the numerous cables with it, speeds of up to 1m/s are achieved over a 4m travel length. At the same time, it was important to remember that this is a public building. The robot must park and retrieve the requested bicycles safely and reliably, as a repair cannot be carried out immediately if the system fails.
SERAAP finally decided on one of our plastic energy chains for medium loads of the E2.1 series. The system was ideal because of its very long service life, which has increased even further compared to the previous model, the E2/000. Another helpful feature for the installation is that the filling and assembly of the chains is quick and therefore cost-saving. Both helped the customer to keep the implementation of the robot cost-effective and thus meet the principal's target price.
Bicycle garage SERAAP during the testing of the bicycle garage: when parked on the platform, the bicycle is locked immediately.
Storage and retrieval unit with energy chain Technical centrepiece: the storage and retrieval unit with E2.1 energy chain for cable guidance


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH