drylin® T - Clearance adjustment

drylin® T linear guide systems always require a minimum clearance between carriage and rail. They are supplied with pre-adjusted clearance ready for installation. For special requirements, please state whether you require an especially narrow or an especially broad clearance. The bearing clearance of the carriages can also be adjusted later if necessary. This should be done without additional load.
manual clearance adjustment drylin T Lateral guide:
- reduce clearance, + increase clearance
manual clearance adjustment drylin T Vertical guide left
manual clearance adjustment drylin T Vertical guide right

This is how it's done:

After removing the protective cover, loosen the locknuts. Width across flats:

SW 5 for TW-01-15 and TW-01-20

SW 7 for TW-01-25 and TW-01-30

Reset the bearing clearance for the 3 guide points with an Allen wrench. Width across flats:

1.5 mm for TW-01-15 and TW-01-20

1.5 mm for TW-01-25 and TW-01-30

After the adjustment, check the clearance of the carriages. If it is adequate, tighten the locknuts and attach protective cover.
In case the clearance has been set too close so that the carriage seizes, it is not enough to reset only the Allen screws. After screwing them back, additionally operate the reset button on the opposite side of the screws to release the gliding elements again. Use a pin of the following size for this purpose:

1.5 mm for TW-01-20 and TW-01-15

3.0 mm for TW-01-25

3.0 mm for TW-01-30




The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH