Harnessed cables for drive technology

Offering more than 5,000 harnessed motor, servo, signal and encoder cables that can be used in energy chains and are suitable for 30 manufacturer standards, igus has the right drive cable for almost any application. The selection of drive cables is so large because there are up to seven cable qualities per cable specification. This is not a one-size-fits all approach; instead, you select the optimum cable based on the application conditions and where the cable is to be used. Whether icy temperatures (as low as -40°C), oil or limited installation space dictate cable selection, the seven cable qualities will enable you to always find the lowest-cost drive cable that works with your application. A guarantee for four years or 100 million energy chain strokes provides additional protection. The third pillar for selecting the right drive cable is the online service life calculator. It takes just a few clicks to calculate the drive cable service life for the application.

Why igus drive cables?

Five reasons to buy igus drive cables


 Individual desired length for each cable, works with 24 manufacturers
 Up to seven cable qualities for optimum selection of the most cost-effective drive cable
Industrial, machine-supported cable harnessing with crimp force and crimp depth monitoring for each cable.
► 14 worldwide networked production sites with standardised processes and high quality 
100% function testing with digital and logic testing for each cable, including a seal of approval a seal of approval

Find the right drive cable quickly with the readycable finder

With 3 clicks to the suitable drive cable

The readycable Product Finder was developed to quickly find the right cable from the large selection (24 drive manufacturers and up to seven cable qualities). In just a few clicks, or by entering the drive manufacturer number, you can use this finder to reduce the selection to a minimum. Finally, choose the quality that is right for your application from one of the seven cable qualities. Nowhere else is this faster or easier.

Get the right plain bearing in just two steps
Find harnessed cables and calculate prices online The readycable® Product Finder is the fastest way to find a drive cable
Go to the readycable® product finder

To the shop for drive cables that work with 24 manufacturer standards

All manufacturers in alphabetical order

Another highlight of this technology is Power over Ethernet (PoE). This allows power to be supplied to the network client over the Ethernet cable. Devices with low power consumption such as VoIP telephones or network cameras can be operated with a single cable thanks to PoE - a separate power supply is not required. This saves costs and reduces the installation effort. The Y-Con Cover 40 was replaced by the Y-Con 40 PP in 2022, which is 100% backwards compatible with the old Y-Con Cover 40.

​​​​​​​More information about Drive Cliq​​​​​​​
Shop for harnessed Drive Cliq cables
Drive Cliq teaser

Already available for these drive manufacturers:
(Bosch Rexroth, Siemens, SEW)

EPLAN macros can save you lots of design and purchasing time because all important information is automatically loaded into the system for you and your colleagues. 

We currently offer EPLAN macros that work with the following drive manufacturers: 
  • Bosch Rexroth
  • SEW
  • Siemens
  • Allen Bradley
  • B&R
  • Beckhoff
  • Fanuc
  • Heidenhain
More about EPLAN macros

Flexible response to order fluctuations

Using igus manufacturing capacities

Challenge us! We are happy to support you in the optimum mix of state-of-the-art manufacturing technology and specialised employees, which in turn frees up resources to support your manufacturing capacities. 

Flexible production planning
Special tools used across projects and customers guarantee consistent quality at low cost. All employees are trained for both readychain assembly and cable harnessing. Flexible production planning secures your delivery times.
Capacities for cable assembly

Reduce the number of suppliers, including to your international manufacturing locations

readycable factories worldwide

igus manufactures more than 12,500 readycables each week at 14 readycable factories around the world. In the Cologne factory alone, 180 people are available to manufacture readychains and readycables. The goal is to reduce transport routes, time, and resources while ensuring consistently high quality. The same production standards apply at all 14 sites.
igus worldwide



The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH