Change Language :

The Polish company Etisoft Smart Solutions develops transport vehicles for material handling. This includes the IntraBot Lift 550 robot, which is an Automated Guided Vehicle (AGV) and part of an intralogistics system that is used for the automated execution of internal transport tasks for components and finished products in a factory or warehouse.
The AGV is designed so that it can be used around the clock and continuously. The robot, which weighs just under 250 kg, has a payload of 550 kg. Due to the payload and uneven floors, the suspension mechanism is exposed to vibrations and high forces. This leads to a load on the mechanical components. For this reason, Etisoft Smart Solutions decided in favour of the use of iglidur® plain bearings.

Shown in yellow: iglidur Z plain bearings and e-chains
The iglidur® Z bearings are used in the wishbones that form the suspension system of the AGVs. The bearings transmit the axial forces that act on the suspension bolts and also enable the entire mechanism to function smoothly. The simple assembly of the igus® products speeds up the manufacturing process of the IntraBot Lift 550. igus® energy chains also proved their worth in the lifting mechanism, protecting the cables during the movement of the mechanism.
In person:
Monday to Friday from 7 am - 17 pm.
Saturdays from 8 am- 12 pm.
Online:
24h
WhatsApp-Service:
Montag – Freitag: 8 – 16 Uhr