Change Language :
The JEEVES service robot can be used for pick-up and delivery services and as a "minibar". There are also a number of smaller applications such as transporting blood samples in hospitals or caring for isolated patients. The sensors of the service robot should be guided safely from the outside to the inside of the robot's drawers without wasting any storage space. Today,narrow E2.10 energy chains enable space-saving and safe cable guidance with a small bend radius, ensuring a long-lasting supply to the moving components even when the drawers are frequently extended.

The JEEVES service robot is mainly used in hotels. Type E2.10 energy chains enable safe cable guiding in the tightest installation space.
Profile
What was needed: Safe guidance of cables, in a very small installation space, from the outside of the robot into the movable drawer.
Requirements: Space-saving, durable, easy-to-install components to facilitate regular cleaning of the robot
Industry: Vending machinery
Success for the customer: The built-in energy chain guides the data cables into the robot safely and without wasting space. The drawers can still be flexibly removed and replaced.