Energy chain above and under water

plastic e-chain® enables maintenance-free operation of tidal turbines in rough seas

Profile

  • What was needed: E4/4 series energy chain; chainflex® motor and signal cable
  • Requirements: The tidal turbine had to be moved reliably and safely over 20 metres in rough seas. Corrosion and climate pose particular challenges for the cable routing, which nevertheless had to be as maintenance-free as possible.
  • Industry: Offshore, renewable energies
  • Success for the customer: The E4/4 plastic chain eliminates the need for any maintenance on the open sea and was the only solution that could be considered, as a conventional metal chain would not have been able to cope with the combination of climate and mechanical requirements.
Floating industrial component with a large white drum on a platform at sea.

Problem

Solution

Large industrial drum with openings on a platform over water.
Long cable chain on a walkway over the water.
Crane boom over water with yellow railing and steel structure.
Black metal structure with a yellow post by the sea.

Products used

Series 4/4 energy chain

igus E4/1 energy chain with closed links for guiding cables and hoses.

chainflex® cable

Several Chainflex cables with different conductor structures in overview.