Smooth movement in the sensor test rig

Profile

  • What was needed: toothed belt axis for conveying the samples between two test sections, a horizontal energy chain to protect the cables on the robot
  • Requirements: long service life, no lubrication or maintenance, simple control system and installation
  • Industry: microelectronics
  • Success for the customer: our toothed belt axes driven by stepper motor from the drylin ZLW series, including the control system, ensure the smooth transport of test parts between two test sections. As the pillow blocks slide over the linear rails without lubrication, no maintenance is required. The linear axis system and the zipper energy chains used on the robot, which protect the cables from wear, help ensure that the automated quality inspection at Hoffmann + Krippner can run without disruption.

Products used

SLW-ES-1040 linear actuator with guide rails and a moving carriage.

Toothed belt axis ZLW

Stepper motor with front flange and connector.

Stepper motor NEMA 23

igus dryve D1 control unit with connectors and status display.

drylin D1 motor control system

igus WJ200UMA plain bearing with metal housing, cut out.

drylin W pillow block

Serie 09 cable carrier with the upper section open.

zipper e-chain

Problem

Solution

"So far, we have always found a solution promptly at igus."

Nico Landeck

Production technologist, Hoffmann + Krippner

drylin gantry robot in a production cell for testing sensor quality.
Drylin axis system with EPSON robot in an automated test setup.
drylin module with a finger pointing to the guide under the device.
drylin slide in a sensor quality test station with cable carrier and measuring setup.