Quiet and failure-free plastic energy chain in container loading crane

As this STS crane works alone, a particularly failure-free roller energy chain was installed.

Profile

  • What was needed: Profile roller e-chain P4
  • Requirements: A quiet e-chain was needed, as the harbour is located near a residential area. As this is the only loading crane at the harbour, the cable routing also had to be absolutely failure-free.
  • Industry: Cranes
  • Success for the customer: The design enables the chain to roll quietly, with the necessary drive force of the e-chain reduced to less than 25%.
A port crane lifts containers at a terminal.

Problem

Solution

Conveyor belt in an industrial plant along a steel structure.