Reach for the sky above Vienna

Profile

  • What was needed: Energy chain series E4.1, chainflex cables
  • Requirements: The cables must be guided safely and reliably at a height of 70 metres – in all weather conditions.
  • Industry: Amusement rides
  • Success for the customer: The chain links are checked every day and no problems have been detected so far.
e-chains on a tall amusement ride against a blue sky.

Problem

Solution

The energy chain is a safety-relevant component, and we can rely on it completely.

Robert Danhel

Technical manager at the Prater Tower

Further impressions of the application

e-chains on the Vienna Giant Ferris wheel with turquoise steel beams and gold details.
e-chains run along a tall steel structure up into the sky.
e-chains guide cables along the steel structure of the Vienna attraction.
e-chains guide cables safely in a vertical installation.