Energy supply systems for the press plant

Robust and quiet at high speed

Large cycle numbers at high speeds and accelerations, large forces, an oily environment: components in the pressing plant must be able to withstand a lot. At the same time, they must meet stringent requirements, since the pressing process must not have downtime, but also be smooth, efficient, and as fast as possible. igus components are designed precisely for such requirements – they are at their best during challenging movements.

Success stories

E-Chain Automotive Strohtmann

Energy safely guided in high-speed sheet feeder

By using linear motor technology, Strothmann GmbH has set new standards in terms of performance and speed. The energy supply with the E6 is perfectly tailored to the high speed and acceleration values and allows a continuous, reliable supply even over longer distances.

Parabolic mirrors from Mithras Holding GmbH

Precise and maintenance-free bearings in rolling machine for mudguards

In a rolling machine for aluminium profiles for the production of lorry mudguards, steel bearings were previously used for the lifting system of the pressure roller. Since these always had to be lubricated and they were not precise in function, they were replaced by completely lubrication-free and maintenance-free drylin linear rails and iglidur plain bearings.


Suitable products

e-chain E6

e-chain system E6

  • For high speeds and accelerations
  • High stability in unsupported and low vibration operation
  • Extremely quiet operation; 46dB(A) depending on speed
Learn more about the E6
chainflex CF113.D

Measuring system cable CF113.D

  • For extremely heavy duty applications
  • Bend radius down to 7.5xd
  • Flame-retardant and notch-resistant
  • Oil-resistant and coolant-resistant
  • PUR outer jacket, PVC-free
More information about the chainflex CF 113.D
chainflex CF27.D

Servo cable CF27.D

  • For extremely heavy duty applications
  • Special pair shielding for 30% faster harnessing
  • Bend radius down to 7.5xd
  • PUR outer jacket, PVC-free
Learn more about the chainflex CF27.D
triflex R readychain

Harnessed dress packs

Consisting of a triflex R e-chain, completely filled with chainflex cables and hoses for the supply of energy, data and media
More information about the dress pack
E4Q e-chain

e-chain system E4Q

  • Can be opened and closed without tools
  • Optional noise dampeners for quieter operation
  • Reduction in material leads to lighter weight
Learn more about the E4Q Series
smart plastics EC.P and EC.B

Condition monitoring for e-chains

  • Sensor EC.P for push/pull force monitoring
  • Sensor EC.B for breakage detection in the initial stage
Find out more about the condition monitoring sensors


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH